AXIS#.SAFEPARAM.SLS_#.FUNCTIONACTIVATION

Description

Indicates whether the Safely Limited Speed (SLS) safety function can be activated. One of the following values can be used:

Value Description

0

Not active

1

Ready for activation

2

Always activated

This function can only be used when a safe encoder is configured in the safety parameters.

 

Parameters Editor with the Function Activation options showing and circled

Context

For complete SLS information refer to SLS (Safely Limited Speed).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1 , 2

Default Value

0 (Never active)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLS_1.FUNCTIONACTIVATION

315ch

01h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_2.FUNCTIONACTIVATION

315dh

01h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_3.FUNCTIONACTIVATION

315eh

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_1.FUNCTIONACTIVATION

325ch

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_2.FUNCTIONACTIVATION

325dh

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_3.FUNCTIONACTIVATION

325eh

01h

Unsigned8

-

-

Read/Write

No